banner

Schneider Electric e-news      |      08/28/2015      |      Schneider Electric Website


Announcing the ArcFM™ Solution 10.2.1a SP1 Release

Schneider Electric is excited to introduce the 10.2.1a SP1 upgrade for the ArcFM Solution. There is no new functionality in the SP1 release, but we've added numerous important bug fixes to many ArcFM Solution applications, including:

  • ArcFM
  • Designer
  • Designer Express
  • Responder
  • ArcFM Server

This release resolves issues discovered by customers in previous versions. For complete descriptions of resolved problems, view the Read Me file that corresponds with each product.

ArcFM Solution 10.2.1a SP1 has been certified against ArcGIS 10.2.1.

ArcFM Solution 10.2.1a and SP1 are certified on Windows 8.1 and Windows Server 2012. Refer to the Supported Versions list in the GIS Support space in exchange for details.

                                              

The installation files for version 10.2.1a SP1 are NOT complete installations. To install 10.2.1a SP1, you must have 10.2.1a installed. Refer to the Read Me file for more information.

All installers are available on exchange in the GIS Downloads group. If you haven't joined the exchange community, simply click Register to get started. You will need to request to join to the GIS Downloads group to access the 10.2.1a SP1 installers.
 


Looking for information about ArcFM Mobile? Visit the ArcFM Mobile space in the exchange community.


To unsubscribe from future versions of Schneider Electric e-news, send a message with Unsubscribe Schneider Electric e-news in the subject line. If you have comments or suggestions concerning Schneider Electric e-news, please email us.