Schneider Electric is pleased to announce the release of Object Reader 10.2.1a for ArcGIS 10.3 for both 32-bit and 64-bit architectures.

 

The ArcFM Object Reader provides visibility to ArcFM custom geo-objects with read-only access to ArcFM data in the geodatabase.  You can only use Object Reader with an ArcFM geodatabase and when you have no other ArcFM Solution product installed.


You can download the zipped .msi files on exchange at Object Reader 10.2.1a for ArcGIS 10.3 (32-bit and 64-bit)