Continuing with our response to customer requests, the numerous performance boosts ArcFM received are now available at 10.1. You'll see substantial improvements in application startup time, opening stored displays, Feeder Manager initialization, and core ArcFM tools such as the Attribute Editor.

 

Designer users will notice considerably better speeds when opening and saving designs, placing template favorites, and using the Designer CU to Work Location Assignment tool.

 

Visit GIS Downloads to access readme files and installers. ArcFM 10.1 applications must be installed prior to installing ArcFM 10.1 QIP patches.