In response to customer requests, ArcFM received numerous performance boosts. You'll see substantial improvements in application startup time, opening stored displays, Feeder Manager initialization, and core ArcFM tools such as the Attribute Editor. We also added one piece of new functionality called Application Metrics. This optional program captures anonymous performance and usage data. The information it collects is enormously useful to our development teams—whose job it is to improve your ArcFM experience.

 

Designer users will notice considerably better speeds when opening and saving designs, placing template favorites, and using the Designer CU to Work Location Assignment tool.

 

ArcFM Server users can also look forward to higher speeds. We're seeing a roughly 50-100% performance improvement in most ArcFM Server operations upgrading from ArcFM 10.1 to ArcFM 10.1.1 QIP (Patch #588).

 

Visit the GIS Downloads place to access readme files and installers. ArcFM 10.1.1 applications must be installed prior to installing ArcFM 10.1.1 QIP patches.