Schneider Electric is excited to introduce the 10.2.1 release of the ArcFM Solution. In response to customer requests, we've focused on making substantial improvements to the performance of ArcFM, Designer, and ArcFM Server.

 

This release also resolves issues discovered by customers in previous versions. For complete descriptions of resolved defects, view the Read Me file that corresponds with each product. You can access Read Me files on the GIS downloads group.

 

ArcFM Solution 10.2.1 has been certified against ArcGIS 10.2.1. The ArcFM 10.2.1 release introduces the following:

 

ArcFM

 

ArcFM received numerous performance boosts:

    • Startup time
    • Core ArcFM tools including the Attribute Editor
    • Feeder Manager initialization
    • Opening Stored Displays

 

We also added one piece of new functionality called Application Metrics. This optional program captures anonymous performance and usage data. The information it collects can be enormously useful to our development teams—whose job it is to improve your experience with ArcFM.

 

Designer

 

Designer users will notice considerably better speeds with each of the following:

    • Open Design
    • Save Design
    • Designer CU to Work Location Assignment tool
    • Placing Template Favorites

 

ArcFM Server

 

We're seeing a roughly 50 - 100% performance improvement in most ArcFM Server operations upgrading from 10.1 to 10.2.1.

 

All documentation is available online at the ArcFM Documentation Center.

 

ArcFM Solution 10.2.1 must be installed with ArcGIS 10.2.1. ArcFM 10.2 applications must be installed prior to installing ArcFM 10.2.1 applications. Refer to the Read Me files for more information.