Welcome to the Pipeline Operation - Natural Gas space on exchange. This area is where you can go to find out general information about our industry leading pipeline operations system, Pipeline Operation, as part of our Enterprise Pipeline Management System.

 

Within each product space you can find information like brochures, whitepapers and case studies. New releases will also be announced here. For customers looking for additional information and support for your Schneider Electric products this can be found on the Oil & Gas Support space (requires login in, for O&G customers only).

 

Additionally many of our product families as part of the Enterprise Pipeline Management System have active Customer Advisory Boards (CAB). Customers are able to join these using the links on the right hand side of each product space where a CAB is active. These CAB spaces are limited to customers of the associated product or solution.