If you have ever wished there was a tool for viewing a configuration or making modifications to the SAGE units without having to be physically connected to one, your wish has come true! The SAGE Off-Line Configuration Tool is now available. The tool requires only a USB dongle to give you the same capabilities for viewing and changing an RTU's configuration that you have when connected to a SAGE unit. Contact your local Rep or Debbie Gierman at 713-920-6897 debbie.gierman@schneider-electric.com for more information.