The full article is in the White Paper section of this site but the short story is this: Red CPU can be used on green or red baseboard without issue. Green CPU can be used on green baseboard without issue. Green CPU on red baseboard needs firmware version F0 or newer.