Want to “OR” alarm points to create a higher level alarm? Boolean Status is an application available in all SAGE RTUs that allows the user to create “And, Or, Nor, Nand, and Xor” gates without using the (IEC 61131 RLL) Ladder Logic Engine. This easy to use application makes it easy to build logic gates.