The Calculation Processor application can be used to compensate for devices that do not send the expected values. For example, an IED that sends analogs in tenths of units. The calculation processor can be used to multiply the value so that it is represented as an integer value.