The C3321 power supply is being replaced with a DIN rail mounted Power Supply arrangement. The new power supply is more compact but has all the same features and connections. See the B1900-D00 and B1900-E00 drawings for connections details.