Make sure you have the right CPU for the firmware you plan to use. The 586 CPU (C3413) firmware (C0 thru E1) has been frozen and is not getting updated with new features. All new features are on the LX800 CPU (C3414) which is otherwise known as the "Red" CPU.