If you've ever used the Data Trap feature of the SAGE Smart RTUs you may have wished it could be viewed in something other then Hex. Well it can! Download the Protolyzer Data Trap/parser tool. It supports DNP and Modbus, Series V and Van Comm Protocols. Protolyzer takes the downloaded Data Trap file and converts them into "English" making the data trap feature built into every SAGE RTU even better for decoding the data stream between devices. Check out the new Protolyzer!  Go to the download page to get this handy FREE tool!