Many Responder users have requested a trace tool that allows them to enter a distance and trace downstream that distance.  The typical use case is that their SCADA system reports a fault on the line a certain distance down from the substation breaker.  They want to be able to type in that distance and have Responder provide them with a set of points that far downstream. 

 

We're offering it as a 'Cool Tool', freely available and usable to any Responder or ArcFM customer.

 

Take a look at it here Cool Tool: Trace by Distance

 

Keith