We are targeting the first week of September to release ArcFM for Silverlight 3.2.  Here's a preview:


Compatibility

  • Compatible with ArcFM Server 10.2.1 and 10.2.1a
  • Compatible with ArcGIS Server 10.2.1 and 10.2.2

 

Contents

  • Upgrade to Esri Silverlight 3.2 and Microsoft Silverlight 5
  • High-resolution server-side printing (see below)
  • Local priority for world address locator
  • Option to ignore ArcFM properties (field alias, field order, etc.)
  • Option to not persist user's selection of visible layers
  • Zoom to full extent fixes
  • Other bug fixes

 

High-Res Printing Features

  • The print button appears along the top of the map next to other common map tools
  • User can choose a specific scale and adjust the extent for the plot in the print preview
  • The plot will have the exact map frame you see in the print preview
  • The plot is processed server-side using the page templates in your geodatabase and ArcGIS print services
  • Admin can configure text fields to be filled in by the user and included in the plot
  • Asynchronous processing so you can continue working after starting the print process
  • High resolution output

 

NOTE

The client-side printing functionality in ArcFM for Silverlight 2.4 will no longer be available in ArcFM for Silverlight 3.2.  We will provide documentation to support migration to high-res server-side printing.