Development begins soon in ArcFM for Silverlight and ArcFM Server for improved printing support!

 

Now is your chance to offer requirements for printing.


plot.png


Note we are are targeting only "essential" support for printing in ArcFM for Silverlight, as the lifetime of Silverlight is limited.  Some essential requirements we have heard so far:

 

  • "One button" printing, that is, minimal clicks required to produce a plot
  • "Wysiwyg" print preview, where the scale and extent of the plot are clear before printing
  • Higher resolution in plots than currently supported

 

Do you agree these are priority requirements?  Do you have others?