A few things to keep in mind about recent and upcoming ArcFM Server/Silverlight releases:


ArcFM Server 10.1

  • ArcFM Server 10.1 is not compatible with Esri's ArcGIS 10.1 SP1


ArcFM Server 10.1.1


ArcFM Server 10.2

  • ArcFM 10.2 was released on September 4th!
  • We're seeing roughly a 50 - 100% performance improvement in most ArcFM Server operations upgrading from 10.1 to 10.2 and applying Patch #273 or newer
  • ArcFM Server 10.2 will support viewing of Feeder Manager 2.0 info with Esri's hot fixes for NIM093448:  QFE-102-S-266424 (ArcGIS 10.2 for Server) and QFE-102-DT-266424 (ArcGIS 10.2 for Desktop)
  • We intend to add support for editing data that causes changes in a Feeder Manager 2.0 network to ArcFM Server 10.2 in the future.


ArcFM for Silverlight

  • ArcFM for Silverlight 2.4 was released in April 2013 and works with ArcFM Server 10.0.3 SP1, 10.1, 10.1.1, or 10.2.  If you are using the Address Search functionality, we recommend changing to the newer geocoding services before December 31, 2013.
  • ArcFM for Silverlight 3.2 is currently planned for late Q3 or Q4 of 2014.  Our focus will be on ensuring compatibility with Version 3.2 of Esri's ArcGIS API for Silverlight and high-resolution printing.  ArcFM for Silverlight 3.2 will require the latest version of ArcFM Server available at the time of its release for full functionality.