Skip navigation
1 2 3 Previous Next

ArcFM Mobile

36 Posts authored by: Jon Fairchild

I’m happy to announce the completion of the first phase of product updates for OIDC! This upgrade process will put our solutions in line with industry standards for security protocols.

 

ArcFM Sync Service OIDC Release

Customers can now begin downloading and installing the upgraded Sync Service. This release is backward compatible so the mobile apps will continue to function. There is no requirement to recreate or re-download replicas. Upgrade instructions are provided here:ArcFM Sync Service 

 

As a reminder, customers must complete the Sync Service upgrade before April 1 to avoid downtime for users!

 

A couple more notes:

  1. You must be on the latest version of ArcFM Solution Center to manage offline data with the Sync Service upgrade. Normally, the Solution Center upgrades itself automatically when you start and restart the application. After restarting, check the About tab in the Solution Center to make sure you have version 1.2.0 or greater. If you do not, install the latest version from here: ArcFM Solution Center
  2. The following capabilities are no longer available in the ArcFM Mobile Portal web app: user management, API key management, and redline type management. Instead, use the ArcFM Solution Center for these items. Also, the “Inspector Sync” tool is no longer available for download as it is obsolete with latest authentication and ArcFM Solution Center capabilities.
  3. You will notice a “Legacy Api Keys” tab in the ArcFM Solution Center. Please ignore this tab for now. There will be additional instructions later about API Key conversion.

Soon the Schneider Electric product development team is releasing an important upgrade to ArcFM Mobile to leverage OpenID Connect, known also as OIDC, for authentication. This includes changes to our hosted services as well as to services and applications installed in your enterprise. This upgrade will put our solutions in line with industry standards for security protocols. As a bonus, this upgrade will also enable a single user to authenticate to multiple tenants for the organization (requested by some ArcFM Mobile customers).

 

Here is the targeted timeline:

 

February 15: ArcFM Sync Service OIDC Release

After this release customers can begin downloading and installing the upgraded Sync Service. This release is backward compatible so the mobile apps will continue to function. There is no requirement to recreate or re-download replicas. Upgrade instructions are provided here:

https://infrastructurecommunity.schneider-electric.com/docs/DOC-7753

 

Customers must complete the Sync Service upgrade before April 1 to avoid downtime for users!

 

April 1: Full OIDC Release

After this release customers can upgrade remaining services and all desktop applications. This release is backward compatible so existing authentication functionality will continue to function.

 

Mobile apps and the ArcFM Solution Center will update automatically. Any customers that have used the controlled rollout feature must “unpin” from earlier releases to allow mobile app upgrade.

 

All other services and applications listed here that you have installed currently must be upgraded according the instructions provided here:

https://infrastructurecommunity.schneider-electric.com/groups/arcfm-mobile-downloads

 

June 1: Non-OIDC Support Ends

After this date any services or applications that have not been upgraded could fail to authenticate!

 

 

Even though this might sound intimidating, I want to emphasize that this is a straightforward upgrade, and the security enhancements justify the effort required. Our support team is ready to assist you and answer questions.

With today's release of ArcFM Mobile 3.4 for Windows, utility-scale construction workflows begin to take shape!

 

This release includes new capabilities to enable the construction as-builting process:

  • Crews can activate work locations in the map from an external workforce management system, and ask for turn-by-turn directions, to get to a day's work more efficiently.
  • Upon completion of a job, the foreman can more effectively communicate as-built changes to assets, map corrections, and field conditions in redlines with attributes.

 

ArcFMMobileRedlineAttributes.png

 

 

To get started with ArcFM Mobile, contact your account manager!

 

The ArcFM Mobile 3.4 for Windows release notes and installer are available here, and your existing users will be upgraded automatically:

ArcFM Mobile for Windows Release Notes

 

For your users to fully benefit from the improvements in ArcFM Mobile for Windows 3.4, you must upgrade the ArcFM Redlining Service and ArcFM Redlining Tools for ArcGIS:

ArcFM Mobile Services and Tools Release Notes

 

Important Note:  If your organization uses BOTH the ArcFM Redlining Tools for ArcGIS and the ArcFM Mobile Tools for ArcGIS on the same machine, you must upgrade both of these applications at the same time or the user will encounter errors when attempting to log into these tools.

ArcFM Mobile Services and Tools Release Notes

 

Also we recommend you upgrade the ArcFM Solution Center for some bug fixes:

ArcFM Solution Center Release Notes

 

#ArcFMMobile  #ArcFM11  #SchneiderGIS #UtilityScaleGIS

Utility-scale mobile GIS just became more so with the release of ArcFM Mobile 3.3 for Windows.

 

This release includes a variety of new and improved capabilities bringing more value to our customers:

 

  • Windows 10 users can request turn-by-turn directions to any point on the ArcFM Mobile map, for reduced travel time to assets and work locations.
  • Gas technicians benefit from workflow enhancements around the ignore valve and squeeze-off options in gas isolation tracing, for improved productivity.
  • Customer administrators now have the option to override the default behavior of automatic application updates to users' devices. The admins can deploy the new app for testing and training before releasing to full production, thus insuring a smooth transition for users to new functionality.
  • ArcFM Mobile for Windows now fully supports map services that are federated with Portal for ArcGIS, improving security around published data.

 

DriveToHere.png

 

ArcFM Mobile for Windows Release Notes

ArcFM Solution Center Release Notes

ArcFM Mobile Services and Tools Release Notes

 

To get started, contact your account manager or visit ArcFM Mobile Jumpstart

 

#ArcFMMobile  #ArcFM11  #SchneiderGIS #UtilityScaleGIS

Are you heading to Chicago next week? It would be great to catch up with you and talk mobile!

 

Here are some opportunities to learn more about ArcFM Mobile at the conference:

 

  • Come to the Schneider Electric booth #302 for a demo of the latest tools including configurable redlining and one-click tracing.
  • Join Jillian Durbin and myself for a look at The Energy Coop's implementation of ArcFM Mobile for improved productivity in gas operations. Friday 9:10 - 9:45 AM in Williford AB

 

EnergyCoopBackhoe.jpg

 

Click here for more details on Schneider Electric's presence at GeoConX

 

#ArcFMMobile  #ArcFM  #SchneiderGIS  #UtilityScaleGIS

This week we have published a minor release of ArcFM Mobile for iPad. The highlight of this version is better visibility of the map while redlining. Users can now view nearby previously-drawn redlines and current GPS location while placing new redlines. Now your field personnel have the context they need to mark up the map efficiently without extra clicks and switches in view. Less clicks make happy users!

 

ArcFMMobileIpad3.1.2cropped.png

 

ArcFM Mobile for iPad Release Notes

ArcFM Mobile for iPad

 

#ArcFMMobile  #ArcFM  #SchneiderGIS  #UtilityScaleGIS

 

Would you like to see a demo of what’s new in ArcFM Mobile for Windows?

 

ArcFMMobileElectricTrace.png

 

Check out our webinar What’s New in ArcFM 10.2.1d and ArcFM Mobile Thursday, July 20 at 11 am MT.

 

More details here:

https://infrastructurecommunity.schneider-electric.com/community/events/gis-events

Today Schneider Electric takes offline mobile GIS to a whole new level with the release of ArcFM Mobile 3.2 for Windows.

 

ArcFM Mobile delivers speed and simplicity to end users and administrators, enables collaboration between field and office, and supports the scale requirements of any size utility.

 

This release of ArcFM Mobile for Windows includes all-new network tracing capabilities:

  • Electric isolation tracing, providing safety and impact information including upstream protective devices, tie points, and downstream affected customers
  • Gas isolation tracing, providing safety and impact information including isolation valves and affected customers, with options to ignore valves and place squeeze-offs
  • A one-click user experience where users just tap an asset and isolation results appear
  • Full offline support so users can trace the network anytime, anywhere, with fast results
  • Minimal configuration by leveraging your existing Feeder Manager implementation

 

 

Also new with this release are configured searches:

  • Google-style searches using minimal text entry in a single box to accelerate the workforce's access to asset data
  • Quick and easy configuration with a few clicks by the admin to enable the searches relevant to each map, thus giving end users only the search tools they need for their job
  • Multiple search targets where a user's search text can be applied to multiple fields and multiple layers, allowing consolidation of search tools
  • Full offline support, of course, because it's ArcFM Mobile!

 

And a few more enhancements:

  • ArcFM Mobile activation from external applications of the device such as WMS, MWFM, and EAM mobile apps, improving integration with enterprise solutions
  • New and improved configuration docs, organized by configuration workflow to accelerate implementation
  • And introducing the ArcFM Solution Center for inituitive, centralized configuration of the ArcFM ecosystem

 

 

To get started, contact your account manager or visitArcFM Mobile Jumpstart

 

ArcFM Mobile for Windows Release Notes

ArcFM Mobile Services and Tools Release Notes

 

#ArcFMMobile  #ArcFM11  #SchneiderGIS #UtilityScaleGIS

This week we have published a minor release. The highlight of the latest version is a "hideable" list of callout content as part of redlining. This allows field users to quickly view the text for all visible callouts with a single click, and then hide it with another click. Less clicks means happier users!

 

ArcFMMobileRedliningWithCalloutList.png

 

ArcFM Mobile for Windows Release Notes

ArcFM Mobile for Windows

 

#ArcFMMobile  #ArcFM  #SchneiderGIS  #UtilityScaleGIS

Are you coming to Fort Collins for Link at the end of February? I hope so!

 

We have a lot of exciting advancements in ArcFM Mobile to share with you, including:

 

  • ArcFM Mobile’s rapid advance to fulfill its role in the ArcFM Solution XI ecosystem as the tool for field crews in design/build workflows.
  • December’s release of redlining workflows in ArcFM Mobile for Windows, featuring extreme usability for crews and redlining palettes configurable for your organization's requirements.
  • Partially or fully disconnected capabilities for any number of mobile users, thanks to the scalable ArcFM Sync Services. Next up is offline network tracing for both electric and gas networks.

 

ArcFMMobileElectricTrace.png

 

You’ll see more at the opening day sessions, the Marketplace, and at several sessions:

 

  • Better ROI with ArcFM Mobile - A Technical Perspective
  • Enabling Your Business with Utility-Scale ArcFM Mobile, with Southern Company
  • Happy Linemen and Easy Admin with Offline ArcFM Mobile, with City of Vero Beach

 

Link 2017

 

Safe travels!

 

 

#ArcFMMobile  #ArcFM  #SchneiderGIS  #UtilityScaleGIS

Have you registered?

 

Here's your chance to learn about new capabilities in our December 2016 releases.

  • ArcFM Web 4.6.2
  • ArcFM Mobile 3.1 for Windows

 

Thursday, January 12, 11am MST

 

Webinar: What's New in ArcFM Mobile and ArcFM Web!

 

Video now available: What's New? ArcFM Mobile and ArcFM Web

 

NewArcFM-Masthead-Image.jpg

 

Hope to see you there!

Today Schneider Electric raises the bar for mobile GIS once again with the release of ArcFM Mobile 3.1 for Windows.

 

ArcFM Mobile delivers speed and simplicity to end users and administrators, enables collaboration between field and office, and supports the scale requirements of any size utility.

 

What's the ArcFM Mobile difference that makes it the utility-scale mobile GIS solution?

  • Rock-solid, fast, and scalable offline capabilities that are unique in the market of Esri-based mobile GIS solutions
  • Extreme usability of apps allowing the utility workforce to focus on their job instead of software
  • Guaranteed to work in the ArcFM ecosystem out of the box. That's why it's called ArcFM Mobile!

 

This release of ArcFM Mobile for Windows includes all-new redlining capabilities:

  • A fast and simple user experience where crews just place redline graphics - no GIS experience or training is required
  • Configurable for your organization to build custom redlining palettes, optionally including your asset symbology
  • Full offline support so users can create redlines anytime/anywhere, synced to the enterprise automatically when a connection is available
  • Workflow support bringing redlines to ArcFM Desktop for processing; and they can be viewed on any ArcGIS Platform app as well!

 

ArcFMRedlineTools_Short.png

 

Those of you who have joined the ArcFM Mobile PAG can have a look at ArcFM Mobile redlining in this preview demo.

 

To get started, contact your account manager or visit ArcFM Mobile Jumpstart

 

 

#ArcFMMobile  #ArcFM  #SchneiderGIS #UtilityScaleGIS

Next month, our utility-scale mobile GIS gets even better with the release of ArcFM Mobile 3.1 for Windows. The primary new capability is redlining. Not just any redlining, but the Cadillac of redlining solutions! Capabilities include:

 

  • Redlining palettes that can be configured to meet your organization's needs, including the use of your asset symbology
  • A fast and simple user experience where crews simply place redline graphics - no GIS experience or training required
  • Full offline support - create redlines anytime/anywhere and they are synced to the enterprise automatically when a connection is available
  • Redlining workflows bring sketches to ArcFM Desktop for processing; and redlines can be viewed in any ArcGIS Platform app as well

 

Those of you who have joined the ArcFM Mobile PAG can have a look at ArcFM Mobile redlining in this preview demo.

 

ArcFMMobileRedliningWithPalette.png

 


Stay tuned for the release of ArcFM Mobile 3.1 for Windows next month!

 

#ArcFMMobile  #ArcFM  #SchneiderGIS #UtilityScaleGIS

A new release of Schneider Electric's scalable, multi-platform, mobile GIS solution is coming soon... It includes the addition of intuitive, configurable redlining capabilities to ArcFM Mobile for Windows. For an early look, drop by booth 300 and ask for a demo!

 

ArcFM Mobile Redline Palette.png

 

Also you can see ArcFM Mobile in action for your user colleagues... Learn about Southern Company's mobile GIS business drivers and the results of their ArcFM Mobile pilot at this session:

 

Enabling your Business with Utility-Scale Mobile GIS

Wednesday, Oct. 19 in room Sunset A/B

 

Hope to see you in Phoenix!

 

#ArcFMMobile  #ArcFM  #SchneiderGIS #UtilityScaleGIS

Today Schneider Electric sets a new standard for scalable, multi-platform, mobile GIS solutions with the release of ArcFM Mobile 3.0 for Windows!

 

ArcFM Mobile delivers the advantages of speed and simplicity. It provides instant, intuitive access to data for your workforce wherever they are, while meeting the scale requirements of the largest utility and communications providers.

 

Features include:

  • An intuitive native app for Windows 7, 8, and 10, so your workforce can access the GIS on their current devices and be productive with little or no training
  • Optimized asset viewing and identification, including related objects, to make information instantly available to users regardless of connectivity
  • Screaming fast Google-style searches that recognize proximity to the user’s location, so users never wait for the most relevant results
  • Scalable offline map download and synchronization, backed by the powerful ArcFM Sync Services, to support gigabytes of data and hundreds or thousands of users
  • Easy management of offline content in a single configuration site for both iPad and Windows users, minimizing administration costs
  • “App-store” style deployment, enabling implementation across your workforce in days rather than months

 

 

Also, ArcFM Mobile 3.1 for iPad is now available, including:

  • An "offline maps" toggle to view only downloaded map data, improving app performance and reducing data costs
  • Improved usability around partial connectivity and map download/synchronization
  • Many user interface improvements and bug fixes

 

For more information, see 2016 Q2 ArcFM Mobile Release Notes and 2016 Q2 ArcFM Mobile Services, Portal, and Tools Release Notes.

 

To get started, contact your account manager or visit ArcFM Mobile Jumpstart

 

#ArcFMMobile  #ArcFM  #SchneiderGIS #UtilityScaleGIS