Some exciting improvements are coming with the release of ArcFM Mobile 3.0, scheduled for the end of February!  This includes the industry's most advanced technology for offline data management:


  • GIS administrators at utilities can easily prepare GIS data for offline use, optionally organized by region.
  • Offline data can be downloaded to devices and changes to the enterprise GIS can be quickly synchronized.
  • The technology handles gigabyte-scale data and hundreds of users to support the largest of utilities.


With ArcFM Mobile 3.0, your workforce can always have instant access to the latest asset GIS information and stay productive regardless of connectivity.




Stay tuned for more news on ArcFM Mobile 3.0.  And come check it out at Link 2016.  There will be demos and discussion of offline data management throughout the conference.  These two sessions will address the technology in detail:


  • Strategies for Success in Enterprise Mobile - Wednesday, March 2, 2016, 2:00 pm
  • Rutherford EMC Goes Offline with ArcFM Mobile - Thursday, March 3, 2016, 10:40 am


Hope to see you there!


#ArcFMMobile  #ArcFM  #SchneiderGIS #UtilityScaleGIS