Skip navigation
2014

Release 1.6 of Orbit Mobile for Windows and iPad is now available!  This is primarily a performance and stability release.  Here are a few highlights since last month's Release 1.5:

 

• Significantly reduced the time it takes to initially load as well as refresh the task list.  Also, the load and refresh times are now more consistent.
• Scrolling within the iPad app is now more responsive.
• With the iPad app, you can now perform a double-tap to identify features on the map.

 

Note: Release 1.6 of the Orbit Mobile for Windows was patched on 10/03/2014 with performance enhancements and bug fixes.