I am pleased to announce Release 1.4 of ArcFM Mobile Mobile for Windows and iPad!  We've added a number of new features while maintaining cross-platform parity between the Windows and iPad versions of the app.


Here are some of the improvements we've made:

• Ability to search and identify features in ArcGIS for Server map services
• During ad-hoc task creation, feature attributes are copied from ArcGIS for Server into the new task’s properties if the field names are the same
• Also, default field values configured in Orbit Portal are copied into the new task’s properties
• Store latitude and longitude (referenced to WGS 84) for tasks created on features
• Additional task filtering:  Task Type and Today
• Provide status for tile packages that are downloading in the background
• Improved support for a variety of Active Directory Federation Services (AD FS) configurations
• Alignment with iOS 7 look and functionality


Orbit Mobile for Windows

Win_4_Small.png  Win_3_Small.png


Orbit Mobile for iPad

iPad_4_Small.png  iPad_3_Small.png