I’ve got multiple cable features available in Fiber Cable feature class.  Now I would like to create the associated Buffer Tubes and associated Fibers for all of the Cables.  Instead of manually creating I would like to automate it through a piece of code.  In the process I was searching in Fiber Manager API for the appropriate Classes, but no luck. Can anybody have a clue on what classes/interfaces available for creating Buffer Tubes/Fibers.  By the way, I’m working on 10.2.1a.

 

Regards,

Kranti